AXIS#.SAFEPARAM.SBT.MAXMOTIONBRAKE#
Description
Indicates the amount of rotation that should occur for the shaft attached to the specified brake. If the amount of motion detected is larger than this specified amount, the Safe Brake Test (SBT) will enter a failed state and the Safe Brake Acknowledge (SBA) signal is low.
The drive will still be allowed to be enabled and command motion. It is up to the safety system to prevent motion in the event of a failed/expired SBT (ie: SBA signal). |
Context
For complete SBT information refer to SBT (Safe Brake Test).
Related safety parameters:
- AXIS#.SAFE.SBT.ERROR
- AXIS#.SAFE.SBT.MOVE
- AXIS#.SAFEPARAM.SBT.MAXAPPLOAD
- AXIS#.SAFEPARAM.SBT.MAXTIMEINTERVAL
- AXIS#.SAFEPARAM.SBT.TORQUEDURATION
- BRAKE#.SAFE.SBT.ELAPSED
- BRAKE#.SAFE.SBT.STATE
Versions
Action |
Version |
Notes |
---|---|---|
Implemented |
02-01-02-000 |
|
General Information
Type |
Read/Write |
Units |
Arc minutes |
Range* |
1 to 4294967295 arc minutes |
Default Value |
300 arc minutes |
Data Type |
Integer |
Stored in Non-Volatile Memory |
No |
*Note: MAXMOTIONBRAKE cannot be set to a greater or equal value than 10800 arcminute. Otherwise, the SMM will return an error code once SBT function is started. The error code can be read by the keyword AXIS#.SAFE.SBT.ERROR, which will report “0x6 – SMM System Error”.
Fieldbus Information
Command |
Index |
SubIndex |
Data Type |
Units |
Float Scale |
Access |
PDO Mappable |
---|---|---|---|---|---|---|---|
AXIS1.SAFEPARAM.SBT.MAXMOTIONBRAKE1 |
3157h |
04h |
Unsigned32 |
- |
- |
Read/Write |
No |
AXIS1.SAFEPARAM.SBT.MAXMOTIONBRAKE2 |
3157h |
05h |
Unsigned32 |
- |
- |
Read/Write |
No |
AXIS2.SAFEPARAM.SBT.MAXMOTIONBRAKE1 |
3257h |
04h |
Unsigned32 |
- |
- |
Read/Write |
No |
AXIS2.SAFEPARAM.SBT.MAXMOTIONBRAKE2 |
3257h |
05h |
Unsigned32 |
- |
- |
Read/Write |
No |